SMS Message ID (Set ID)

Associated with: SCADAPack 50 Outstations.

This status attribute uniquely identifies an individual SMS message in a set of SMS messages sent by Geo SCADA Expert to the device. The attribute has two parts:

Example:

The SMS Message ID might be 300.

The Set ID might be 250.

The Status display would show the attribute as 300 (250).

Below this attribute, the Status display shows information about the SMS message and about its content (see Number of Outstanding SMS Requests).


Disclaimer

Geo SCADA Expert 2022